SLAU846B June 2023 – November 2024 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1519 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3519
The read verify command can be used to read a flash location and compare the data to data which is preloaded into the CMDDATA registers of the flash controller. The command can be applied to a single flash word, multiple flash words (if the device supports multi-word programming), an entire sector, or an entire bank. When performing a read verify on an entire sector or bank, the data in CMDDATAx will be re-used.