SLAU857A May 2021 – July 2021 MSP430FR2476 , MSP430FR2512 , MSP430FR2522 , MSP430FR2532 , MSP430FR2533 , MSP430FR2632 , MSP430FR2633 , MSP430FR2672 , MSP430FR2673 , MSP430FR2675 , MSP430FR2676
CapTIvate, MSP430, and Code Composer Studio are trademarks of Texas Instruments Incorporated.
All trademarks are the property of their respective owners.
Physical button, knobs, and sliders experience the following shortcomings compared to capacitive touch controls. Physical controls:
TI CapTIvate™ capacitive touch technology supports five sensor types: buttons, proximity sensors, scroll wheels, sliders, and touch panels, and a variety of covering materials. CapTIvate technology supports low power consumption, strong and stable induction technology, strong anti-noise ability, and allows for waterproof construction.
This document helps with the capacitive touch development process and helps you quickly understand the full features of TI CapTIvate capacitive touch technology.
Term | Definition |
---|---|
Base capacitance | The parasitic capacitance of the sensor before the finger touches it |
BSL | Bootloader |
CAP I/O | A pin on an MSP430™ MCU that is dedicated to the capacitive touch function |
CapTIvate | TI’s capacitive touch design system |
FRAM | Ferroelectric RAM (also FeRAM or F-RAM) |
GUI | Graphical user interface |
IDE | Integrated development environment |
JTAG | JTAG (named after the Joint Test Action Group) is an industry standard for verifying designs, testing printed circuit boards programming and debugging after manufacture |
LPM0, LPM3, LPM4 | Different low-power modes of MSP430 MCUs. For specific power consumption, see the device-specific data sheet. |
MSP | Mixed signal processor |
NVM | Nonvolatile memory |
Rx | In mutual-capacitance mode or self-capacitance mode, the pin or electrode responsible for charging from the parasitic capacitance to the internal reference capacitance of the MCU. |
SBW | 2-wire Spy-Bi-Wire interface, a typical JTAG interface for MSP430 MCUs |
Tx | In mutual-capacitance or self-capacitance mode, the pin or electrode responsible for charging the parasitic capacitance. |
Figure 2-1 shows a common capacitive touch sensor. Sensors typically use copper on the PCB as electrodes. The top layer is covered with a nonconductive protective layer, such as glass or plastic, and glued to the PCB. A grid ground surrounds the sensor.
Based on the type of capacitance detected, capacitive touch can be described as self-capacitive detection (detecting the capacitance value between a single electrode and power line ground) or mutual-capacitive detection (detecting the capacitance value between two electrodes).