SLAU858A november   2021  – june 2023

 

  1.   1
  2.   AFE881H1 Evaluation Module
  3.   Trademarks
  4. 1Overview
    1. 1.1 Kit Contents
    2. 1.2 Related Documentation From Texas Instruments
  5. 2USB2ANY Interface Adapter
    1. 2.1 Signal Definitions for J10
    2. 2.2 USB2ANY Theory of Operation
  6. 3EVM Hardware Overview
    1. 3.1 Electrostatic Discharge Caution
    2. 3.2 EVM Block Diagram
    3. 3.3 EVM Jumper Summary
    4. 3.4 Terminal and Pin Definitions
    5. 3.5 Connecting the USB2ANY
    6. 3.6 Connecting the USB Cable to the USB2ANY Interface Adapter
    7. 3.7 Optional EVM Operations
      1. 3.7.1 Power Configuration
      2. 3.7.2 External SPI and UART Controllers
  7. 4Software Overview
    1. 4.1 Software Installation
    2. 4.2 Launching the Software
    3. 4.3 Software Features
      1. 4.3.1 AFE881H1 Register Page
      2. 4.3.2 High Level Configuration Page
      3. 4.3.3 Using the Python Scripting Tool
  8. 5Schematics, PCB Layout, and Bill of Materials
    1. 5.1 Board Schematic
    2. 5.2 PCB Components Layout
    3. 5.3 Bill of Materials
  9. 6Revision History

Launching the Software

After installation, a shortcut to launch the GUI can be found in the Start menu. If installed in the default directory, the AFE881H1EVM software can also be launched by navigating to the Texas Instruments folder in the Program Files (x86) directory, as Figure 4-2 shows.

GUID-20210619-CA0I-PWVC-K7BN-XCBXRJKN67RB-low.svgFigure 4-2 Launching the AFE881H1EVM GUI

Figure 4-3 shows the GUI after launch. If the USB2ANY controller is not connected to the PC when the software is launched, the GUI defaults to demo mode. Figure 4-4 illustrates the bottom-left corner of the GUI showing the hardware connection status: DEMO MODE or CONNECTED. After the USB2ANY controller is properly connected to the PC, close and reopen the AFE881H1EVM software to detect the device.

GUID-20210619-CA0I-H51J-J10M-Q7ZRBGFDV8VD-low.svgFigure 4-3 AFE881H1EVM GUI at Launch
GUID-1B62E33E-7AAF-40BD-8EF7-84B8ACA168FB-low.gifFigure 4-4 USB2ANY Digital Controller Connection Status