SLAU858A november 2021 – june 2023
To connect the EVM board and the USB2ANY Interface Adapter together, firmly slide the cable ends of the 30-pin ribbon cable into the USB2ANY Interface Adapter and the AFE881H1EVM, as shown in Figure 3-4. Make sure that the connectors are completely pushed together. Loose connections between the USB2ANY and the EVM can cause intermittent operation.