SLAU904A October 2023 – December 2023
For the line input configuration shown in Figure 3-8, the TAx5x42 captures the audio signal provided through RCA terminals J2 (IN1), J3 (IN2) or header J47 or J48. The RCA white connector is connected to the INxP and RCA red connector is connected to the INxM. Depending on differential or single-ended configuration, populate J6 or J7 jumper as described in the Input Jumper Configuration table above accordingly. The input accepted in AC/DC-Coupled mode is a differential 2-VRMS full-scale audio signal and if a single-ended source is used, the 1-VRMS signal is supported.