SLAU913 august 2023 AFE539A4
The SMART-DAC-EVM-GUI incorporates interactive functions that configure an individual AFE539A4EVM device using I2C or SPI communication. These functions are built into several GUI pages, as shown in the following subsections. The menu bar on the far left of the GUI allows the user to switch between pages. The menu bar displays the High Level Configuration page with AFE539A4 sub page, and the Low Level Configuration page.
Before using the GUI, see the device data sheet for detailed AFE539A4EVM programming instructions.