SLAU916 May 2024
The High Level Configuration page is used to set the configuration of the DAC805xxEVM GUI. The page is comprised of two tabs: DAC80516 - DACs and DAC805016 - CLEAR/GPIO. These two tabs act as shortcuts to configure the DAC80516 for basic functionality and testing.
Figure 4-8 shows the DAC80516 - DACs tab of the High Level Configuration page. This tab is used to set the gain and output of the DACs. The internal reference can also be powered on and off here.
Figure 4-9 shows the DAC80516 - CLEAR/GPIO tab from the High Level Configuration page. This tab is used to set the clear values of the DACs, along with setting the configuration for the GPIO pin.