SLAU927B June 2024 – November 2024 MSPM0G3507
Driver Min on time defines the combined rise time and settling time of the current sense amplified output. This value has to be captured independently for a full scale change in voltage across the current shunt. For accurate current sense reading, the current sense amplifier output to be settled before the current signal is captured.
This CSA Settling + Rise time is to be set using #define DRIVER_MIN_ON_TIME_nS macro in the main,h file.