SLAU927B June 2024 – November 2024 MSPM0G3507
Using the motor data sheet, the user can input the motor phase resistance in milliohms (mΩ) using the mtrResist parameter in the System Configuration page. If the motor does not have a data sheet, then measure the phase-to-phase resistance across any two phases using a digital multimeter and calculate the phase resistance by dividing the phase-to-phase resistance by 2 as shown in Resistance Measurement
The motor phase resistance refers to the equivalent phase to center tap resistance, RPH, as shown in Figure 6-2. This measurement is valid for both star wound and delta wound motors.