SLAU927B June 2024 – November 2024 MSPM0G3507
This mode can be selected by setting the CONTROL_MODE in CLOSED_LOOP1 Register as 0h. In speed control mode, the speed of the motor (Electrical Hz) is controlled using a closed loop PI control according to the input reference set as SPEED_CTRL value in Speed Control Register (P.U value in IQ15 format). The P.U speed is computed as the ACTUAL_MOTOR_SPEED / MOTOR_MAX_SPEED value configured in SYSTEM_PARAMETERS.
Example: For MOTOR_MAX_SPEED set to 100Hz , Setting reference Input in SPEED_CTRL to 0x3FFFh (0.5 P.U in IQ15) sets the Motor Speed to 50Hz.