SLAU936 August 2024 TAS2120
TAS2120EVM comes setup for Hardware Mode by default.All the default jumper settings is shown in TAS2120 Mono Evaluation ModuleApplication Diagram for 1S Battery SystemSoftware Mode Jumper SettingsHardware Mode Jumper SettingsDefault Jumper Settings for Hardware Mode.
The default positions for all the jumpers on TAS2120EVM is shown in Table 3-3.
Jumper | Setting | Description |
---|---|---|
SEL1 (J9/J86) |
21dBV-RampEn |
Short from the middle row to a nearby pin to select one of the gain and ramp enable or disable options. |
SEL2 (J10/J87) |
TDM0 / I2SL |
Short from the middle row to a nearby pin to select one of the channel options. |
SEL3 (J78) |
Falling Edge |
Select SBCLK sampling edge. |
SEL4 (J79) |
80mW |
Select the Y-Bridge Threshold option. |
SEL5 (J8/J12) |
1S Mode |
Select 1S power mode. 2S mode requires special power connections. |
IOVDD_BUFF (J40/J43) |
IOVDD_MB |
Set IOVDD_BUFF rail to be same as IOVDD_MB. |
J54 |
Open |
EEPROM Address. |
J53 |
Short |
EEPROM WP. |
J59 |
Open |
Additional SDA pull-up. |
J61 |
Open |
Additional SCL pull-up. |
VBAT (U1) (J5) |
VIN (J21) |
VBAT pin on TAS2120 powered from J21, refer to Section 3.7. |
VBAT_SNS (J4) |
GND |
VBAT_SNS pin connected to GND. |
J3 |
Short |
IOVDD powered from IOVDD_MB when shorted, refer to Section 3.5. |
J7 |
Short |
AVDD powered from on-board 1.8V LDO when shorted, refer to Section 3.6. |