Two mono EVMs can be interconnected using J2 and J6 headers, place the EVMs side by side and connect J6 from the first EVM to J2 on the second EVM.
CAUTION: When 2 EVMs are
interconnected, both EVMs must be set to the same mode, that is, either both EVMs
are in Hardware mode or both EVMs are in Software mode. Mixed configuration is not
supported. Use the same jumper settings for both EVMs.
CAUTION: If using Hardware
mode for 2-Channel configuration, then R19 located in the center of the bottom side
of the PCB must be removed from the EVM to isolate SEL2 for each EVM.