SLAU944 August 2024 TAS2320
TAS2320EVM has been designed such that the dummy load or speaker load connected to the device can be measured very accurately directly from the device pin including board parasitic and connector contact resistance using 4-wire method in digital multimeter. Pin header have been provided to be able to connect digital multimeter in 4-wire mode as shown in Figure 3-9.
Connect HI of DMM to pin-1 and HI_SNS of DMM to pin-2 of TP19 test point.
Connect LO of DMM to pin-2 and LO_SNS of DMM to pin-1 of TP20 test point.