For applications that require stopping the motor
quickly, configure Motor stop options [MTR_STOP]
to either Low side braking:
- Configure Motor stop options [MTR_STOP] to Low
side braking.
- Select Speed threshold for BRAKE pin and Motor
STOP options. Setting speed threshold to higher
speed can result in FETs carrying large current.
Setting speed threshold to lower speed results in
increase in the stop time of the motor.
Recommended to start with 50% of the maximum
speed, If the motor phase current exceeds the FET
maximum current rating, then decrease the
threshold. If the stop time is too high, then
recommended to increase the threshold without
hitting the maximum current limit.