Advisories that affect the device's operation, function, or parametrics.
✓ The check mark indicates that the issue is present in the specified revision.
Errata Number | Rev J | Rev I | Rev H |
---|---|---|---|
COMP3 | ✓ | ||
CPU44 | ✓ | ✓ | ✓ |
FLASH19 | ✓ | ✓ | ✓ |
FLASH24 | ✓ | ✓ | ✓ |
FLASH25 | ✓ | ||
FLASH27 | ✓ | ✓ | ✓ |
FLASH36 | ✓ | ✓ | ✓ |
FLL4 | ✓ | ✓ | ✓ |
FLL5 | ✓ | ✓ | ✓ |
FLL6 | ✓ | ✓ | ✓ |
FLL7 | ✓ | ✓ | ✓ |
LCDA5 | ✓ | ✓ | ✓ |
LCDA7 | ✓ | ✓ | ✓ |
SDA4 | ✓ | ✓ | ✓ |
TA12 | ✓ | ✓ | ✓ |
TA16 | ✓ | ✓ | ✓ |
TA21 | ✓ | ✓ | ✓ |
TAB22 | ✓ | ✓ | ✓ |
TB2 | ✓ | ✓ | ✓ |
TB16 | ✓ | ✓ | ✓ |
TB24 | ✓ | ✓ | ✓ |
USCI15 | ✓ | ✓ | ✓ |
USCI19 | ✓ | ✓ | ✓ |
USCI20 | ✓ | ✓ | ✓ |
USCI21 | ✓ | ✓ | ✓ |
USCI22 | ✓ | ✓ | ✓ |
USCI23 | ✓ | ✓ | ✓ |
USCI24 | ✓ | ✓ | ✓ |
USCI25 | ✓ | ✓ | ✓ |
USCI26 | ✓ | ✓ | ✓ |
USCI28 | ✓ | ✓ | ✓ |
USCI30 | ✓ | ✓ | ✓ |
USCI34 | ✓ | ✓ | ✓ |
USCI35 | ✓ | ✓ | ✓ |
USCI40 | ✓ | ✓ | ✓ |
XOSC5 | ✓ | ✓ | ✓ |
XOSC8 | ✓ | ✓ | |
XOSC9 | ✓ | ✓ | ✓ |
Advisories that affect factory-programmed software.
✓ The check mark indicates that the issue is present in the specified revision.
The device does not have any errata for this category.