SLIA096 January 2022 DRV5021 , DRV5021-Q1 , DRV5023 , DRV5023-Q1 , DRV5032 , DRV5033 , DRV5033-Q1 , TMAG5123 , TMAG5123-Q1 , TMAG5124 , TMAG5124-Q1 , TMAG5131-Q1 , TMAG5231 , TMAG5328
The layout consists of four rocker switch locations placed similar to what might be seen in some automotive door window modules. Each location has two Hall-effect switches, one switch for active rocker lowered left and another for active rocker lowered right. With each rocker switch, there are 3 LEDs: two for the active states and one for the default inactive state. The inactive state LED is driven by an XOR that outputs low when both Hall-effect switch outputs are high.