SLIU024 April 2022 DRV5033 , DRV5033
This EVM allows the user to evaluate Hall-effect switches in a rocker switch application. The EVM includes three rocker switches designed with either the DRV5033FAQDBZ, DRV5033AJQDBZ, or DRV5032ZEDBZ according to the steps described in the HMI Rocker Switch with Hall-Effect Switches application report. In addition to these switches, there is space for incorporating another switch of the user's own design in the quadrant designated as Rocker Switch 4. This rocker switch location provides the user with the flexibility to offset the device from the default location used for the other switches. The EVM is intended to provide basic functional evaluation of the devices. The layout is not intended to be a model for the target circuit, nor is it laid out for electromagnetic compatibility (EMC) testing.