SLLA486B May   2020  – October 2024 ISO1042 , ISO1042-Q1 , ISO1044 , ISO1050 , ISOW1044

 

  1.   1
  2.   Top Design Questions About Isolated CAN Bus Design
  3.   Trademarks
  4. When Do I Need to Isolate CAN?
  5. What are the Options Available to Isolate CAN Bus?
  6. Now That I Have Isolated CAN Signal Path, How Do I Generate Isolated Power?
  7. What’s the Reason Behind Terminating the Bus, Do I Need it, and How to Achieve it?
  8. What’s the Difference Between Common Mode Range and Bus Standoff Mentioned in Data Sheet?
  9. Now That I Have Taken Care of the Termination Resistor, What Other Components do I Need on the Bus Side?
  10. When Connecting Isolated CAN Nodes in a Network, What Should be Done with the Floating Bus-Side Ground Connection?
  11. Is There a Limitation on Minimum Data Rate That I Can Operate? What About the Maximum Data Rate Achievable in a Network?
  12. Is There a Limit on Maximum Number of Nodes That I Can Connect in CAN Network?
  13. 10What Factors Decide the Maximum Communication Distance in a CAN Network?
  14. 11What is the Maximum Value of Bus Capacitance That Can be Introduced Between CANH to GND and CANL to GND? Can Higher Capacitance Damage the Device?
  15. 12Is There a Way to Extend the Maximum Communication Distance?
  16. 13What is Stub Length? What are the Design Considerations Around it?
  17. 14I am Seeing Larger Differential CAN Voltage for Some Bits of CAN Packet Compared to Rest of the Packet When I am Communicating in a Network with Multiple Nodes Connected. Why?
  18. 15References
  19. 16Revision History

Revision History

Changes from Revision A (May 2021) to Revision B (October 2024)

  • Updated the numbering format for tables, figures, and cross-references throughout the documentGo
  • Added opto-emulator and ISOM8610 references where opto-coupler is used throughout the documentGo
  • Changed Software-Controlled Termination Using ISOM8610 image to include ISOM8610Go
  • Changed equation 2 to 3×R×C <=0.75× Bit time(T) Go

Changes from Revision * (May 2020) to Revision A (May 2021)

  • Added ISOW1044 throughout documentGo
  • Updated Isolation Signal and Power Using Small form-Factor ISOW8721 imageGo