SLLA529 October 2020 ISO7741
The considerations for isolated power are similar as for group isolated modules. The isolated power supplies operate with very low currents (in the range of 10 mA), so efficiency at light loads is important. In some designs, the 24-V field supply needed for the analog sensors is provided by the analog input module itself, in which case the isolated power supply must also generate 24 V.