SLLU348 April 2022 TCAN1167-Q1
The RXD output pin is how messages are received from the bus through the transceiver. RXD can be accessed using the main digital IO jumper. There is an optional pull-up resistor for this signal that may be populated to bias the pin state when the signal driver is not active. There is also a footprint for a filter capacitor if desired by the user.