All trademarks are the property of their respective owners.
The TUSB1004EVM is a PCB created to help for customers to evaluate the TUSB1004. The EVM has two Mirco-B USB receptacles and a stacked dual port USB-A receptacle. The user of the EVM can insert a standard Micro-B USB cable into the TUSB1004EVM board then conenct the cable to a motherboard or system. The user can then insert an USB device directly or through an standard USB cable into the USB-A receptacle side of the EVM board.
The following are the major components of the EVM:
Two Micro-B USB receptacle