SLLU359A december   2022  – may 2023

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Cautions and Warnings
  5. 2Introduction
  6. 3Quick Start Guide
  7. 4Hardware and Software Overview
    1. 4.1 Hardware Connections Overview – MCT8329EVM
    2. 4.2 Connection Details
    3. 4.3 MSP430FR2355 Microcontroller & User Interface
    4. 4.4 LED Lights
    5. 4.5 User-Configurable Settings
  8. 5Hardware Setup
  9. 6MCT8329 GUI Application
    1. 6.1 Running the GUI
    2. 6.2 Offline Installer
  10. 7MSP430FR2355 Interface Firmware
    1. 7.1 Downloading Code Composer Studio and Importing MSP430FR2355 Interface Firmware Code
    2. 7.2 Using the eZ-FET to Program the MSP430FR2355
  11. 8Schematics
    1. 8.1 Main Supply
    2. 8.2 Connectors and Interface
    3. 8.3 USB to UART
    4. 8.4 MCU Programming and Debug
    5. 8.5 MSP430FR2355 MCU
    6. 8.6 MCT8329 3-Phase Sensorless Trapezoidal Gate Driver
    7. 8.7 Status LEDs
    8. 8.8 Switches and Speed Input
  12. 9Revision History

Downloading Code Composer Studio and Importing MSP430FR2355 Interface Firmware Code

  1. Extract the “MCT8329EVM_MSP430FR2355_Firmware_GUI.zip” to a location on the computer.
  2. Download the latest version of Code Composer Studio. This download sets up a ti folder in the directory C:\ti.
    1. Accept all agreements, default install locations, and hit Next to proceed through menus.
    2. In the Select Components window, make sure to check MSP430 Low-Power MCUs to install the required packages for the MSP430 LaunchPad Evaluation Kits.
  3. After installing, run CCS and select a folder or the default to use as the Workspace to store any new projects. The location and naming convention can be changed based on the user's preference. Click the OK button to accept.
  4. In CCS, click on the Project tab and select Import CCS Projects. Click on Browse.
  5. Select the MCT8329EVM_MSP430FR2355_Firmware_GUI folder installed from step 1.
  6. Import the project MCT8329EVM_MSP430FR2355_Firmware_GUI into your workspace as shown in Figure 7-1.
GUID-20210823-SS0I-PV51-8SRW-HGP1FLBXCGDW-low.png Figure 7-1 MSP430FR2355 Interface Firmware Code in Code Composer Studio