SLLU387 August 2024
This document is provided with the MCF8315 customer evaluation module (EVM) as a supplement to the MCF8315C Three-Phase Sensorless-FOC BLDC Motor Driver data sheet. This user's guide details the hardware setup instructions, GUI installation, and usage instructions.
Observe the following cautions and warnings as printed on the EVM board.
HOT SURFACE |
![]() |
Hot surface temperature. The EVM can have high surface temperatures marked by the FIRE triangular symbol on the EVM. Avoid touching the marked hot surface are when driving high currents to prevent potential burn damage. |