SLLU388 November 2024
Switch ID | Purpose | Type | Comment | Installed |
---|---|---|---|---|
S1 |
SBC Reset Switch |
Push Button |
Push to Cause Reset on SBC |
Yes |
S2 |
MCU to SPI Bus Switch |
Dip Switch Array |
Close all switches to connect to MCU. Open all switches for external control. |
Yes |
S3 |
WAKE1 Switch |
Push Button |
If J36 is shunted to pull-up source pushing button will create a high to low transition on WAKE1 |
Yes |
S4 |
WAKE2 Switch |
Push Button |
If J37 is shunted to pull-up source pushing button will create a high to low transition on WAKE2 |
Yes |
S5 |
WAKE3 Switch |
Push Button |
If J38 is shunted to pull-up source pushing button will create a high to low transition on WAKE3 |
Yes |
S6 |
MCU Reset Switch |
Push Button |
Push to Reset MSP430 (U2) |
Yes |