SLOA049D July 2000 – February 2023
Figure 7-1 shows the low-pass MFB filter architecture and the transfer function.
Again, the transfer function looks different from standard form in Equation 17. By substituting , , and , the functions become the same.
Depending on how you use the previous equations, the design process can be simple or tedious. Appendix A shows simplifications that help to ease this process.
The Sallen-Key and MFB circuits shown are second-order low-pass stages that can be used to realize one complex pole pair in the transfer function of a low-pass filter. To make a Butterworth, Bessel, or Chebyshev filter, use the previous substitutions with the standard form equations that come from filter coefficients to find circuit component values.