SLOA290A April   2020  – August 2020 TAS5805M

 

  1.   Trademarks
  2. Introduction
  3. Power Consideration
  4. Power Supply
  5. Speaker Configuration
  6. Performance
  7. Efficiency
  8. Modulation
  9. Feedback
  10. Protection
  11. 10Input
  12. 11Advanced Features
  13. 12Additional Information
  14. 13Revision History

Feedback

Class-D amplifiers vary in their feedback topology. Some devices have an internal integrated closed-loop feedback circuit, some have open-loop, and some are configured to support an external closed-loop feedback circuit. Feedback affects the audio performance and noise of a device. Generally, closed-loop systems outperform open-loop systems. Aside from this, a closed-loop device can provide a more consistent output power even with a varying supply voltage. An open-loop device would decrease its output in case of a battery-powered supply, or vary with unstable power supply. The best example of this is an old-school flashlight, where the light dims overtime as the batteries get weaker. As shown in Figure 8-1 are the results of an experiment where a battery-powered Bluetooth® speaker using TAS5342A was re-wired to use the TPA3221 instead. The test was conducted multiple times using each device with the same results. Beginning with a fully charged battery, pink noise was played and the sound pressure level (SPL) was measured until the speaker stopped playing due to the battery draining. While both devices had a similar average SPL, the closed-loop TPA3221 maintained a constant SPL through shutdown while the open-loop TAS5342A demonstrated a decay correlating with the draining battery voltage.

GUID-158CA713-4E08-4DF2-B13C-4C0991762CDA-low.pngFigure 8-1 Open-loop vs. Closed-loop Amplifiers Powered by Battery

Some devices support further enhancement through the use of a feedback loop created external to the amplifier, in addition to their internal feedback loops. This is referred to as a post-filter feedback loop. For more information on this, visit the TPA324x and TPA325x Post-Filter Feedback application note.