SLOA326 October 2022 TAS2781
The output of the boost converter (PVDDH rail of TAS278x) with and without class-H operation is shown in Figure 3-6 through Figure 3-6. The output of the boost converter is set to a constant voltage when the class-H operation is disabled by disconnecting jumper J14 on the TAS278x EVM. The output voltage of the boost converter follows the envelope of the audio waveform when the class-H operation is enabled.
For all the following test waveforms, the hardware setup is TAS2781 EVM using PPC3, AVDD = IOVDD = 1.8 V, load = 8 Ω + 15 µH, PVDDL = 5 V, boost input = 4.2 V. The following waveforms show the differential output of the TAS278x (OUTP – OUTM) and the PVDDH.