SLOA326 October 2022 TAS2781
The connections for the Hybrid-Pro PWM output (PWM_CTRL pin) of the TAS278x and the FB pin of the boost converter are shown in Figure 3-1. The boost converter chosen for the TAS278x EVM is TPS61089. The passive 2nd order low-pass filter converts the PWM signal from the audio amplifier into a DC voltage at the FB pin of the boost converter to control the boost output.