The Temperature Sensing (TS) function is a vital function for providing batteries charge and to operate within a safe temperature range. The BQ25180 provides a TS design as a current source that biases a resistor network with an NTC thermistor. Although the TS is designed to work with NTC of particular characteristics, external resistors extend the NTCs which can be used with the BQ25180. The External NTC Monitoring Calculator, which is available on the TI-Charger GUI, provides an easy means to check the configured application's expected TS behavior.
All trademarks are the property of their respective owners.
Temperature sensing of the battery is a precautionary measure to maintain the battery within safe temperatures during the course of charging. Temperature sensing feature makes use of temperature sensitive resistivity to approximate and respond to battery temperatures while charging. For this purpose, many battery manufacturers incorporate a Negative Temperature Coefficient thermistor into the battery pack; for those battery packs that do not have a thermistor, we recommend including an external NTC alongside the battery pack.
The Japanese Electronics and Information Technology Industries Association (JEITA) guidelines for improving battery charging safety outline a series of battery temperature thresholds which can affect the charging parameters when crossed. These thresholds are typically defined as: cold temperatures below 0°C, cool temperatures below 10°C but above 0°C, warm temperatures above 45°C but below 60°C, and hot temperatures above 60°C. The prescribed behavior for the temperatures below the cold threshold and above the hot threshold is to cease charging until battery temperature has normalized. For battery temperatures in the cool and warm regions charge current and maximum charge voltage can be reduced. Different guidelines apply to different applications, we recommend checking the specific guidelines that apply to a given battery pack.
The operation and configurability of the TS function varies from charger to charger. The BQ25180’s TS function is implemented as a current driven TS sensing. This means that a fixed current source biases an external resistor network placed at the TS pin with ITS_BIAS. The NTC’s temperature dependent resistance correlates the resistance, and therefore voltage, at the TS pin with the battery pack temperature. This voltage is then compared with a series of reference voltages to determine the temperature range within which the battery pack is operating. Although these reference voltages are tuned to work with NTC thermistors with a specific Beta (β) and calibrated impedance, additional resistors can be placed to allow the use of NTCs with different β values and calibrated impedance with minimal error. The TS application is described in Figure 1-2.
The series resistor (RS) and parallel resistor (Rp) can be calculated using a few formulas. The resistance of an NTC thermistor is governed by Equation 1:
RCAL is the resistance of the thermistor calibrated at TCAL, typically 25°C. β is given in terms of Kelvin so T1 and TCAL are expressed in Kelvin. This equation allows us to calculate the thermistor resistance at different temperatures, notably at the HOT JEITA threshold of 60°C (RH) and at the COLD JEITA threshold 0°C (RC). The resistor network and bias current of the TS current source produce a voltage calculated by Equation 2:
The charger data sheet provides voltage thresholds for the various JEITA temperature thresholds. These voltages, in place of VTS, in Equation 2 allows the use of a system of equations to solve for the two variables needed to create our TS circuit: RP and RS. Because there are only have two variables to compensate the system with, only two JEITA thresholds can be met with total accuracy. Typically, HOT JEITA threshold (VH) and COLD JEITA threshold (VC) are prioritized.
Using known values VH, VC, RH, and RC, as well as Equation 2, we create and provide a system of equations to derive Equation 3 and Equation 4 to calculate RS and RP.
The BQ25180 implements a 38 uA current source for biasing the resistor network. The voltage thresholds are tuned to work with a thermistor with a β of 3435 that is calibrated to 10 k Ω at 25°C. As mentioned before, external resistors can be used to allow the BQ25180 to work with other NTCs. Additionally, the BQ25180 allows for adjustable HOT and COLD voltage thresholds for applications which require different ranges. The COOL and WARM thresholds can selectively be disabled through I2C.
TI offers the External NTC Monitoring (TS) Calculator for the BQ25180 to facilitate configuration checking. This calculator can be accessed by selecting the calculator icon from the left menu bar on the BQ25180 TI Charger GUI page.
The planned NTC’s specifications can be entered as well as any calculated RS values, RP values, and register configurations. Once all configuration specifications have been entered, pressing the calculate button populates the outputs with the expected temperatures in Celsius at which the device is expected to enter and exit JEITA thresholds.