SLUAAL7 September 2022 BQ35100
It is difficult to gauge the remaining capacity of a lithium thionyl chloride battery because of the extremely flat open circuit voltage. However, the BQ35100 configured in EOS mode solves this challenge by using impedance data measured during short current pulses. This test shows the data that the BQ35100 can collect, and how that data is used to determine when a lithium thionyl chloride battery is nearing the end of life.