SLUAAM4 December 2023 BQ76905 , BQ76907
The default settings for the BQ7690x devices have COV (over-voltage), SCD (short-circuit), and REGOUT (LDO output) protections enabled. This is verified in the following by reading from the Enabled Protections A register shown in Table 3-9. In Figure 3-1, the value returned from the RAM address 0x9024 is 0xA1.
Class | Subclass | Name | Type | Min | Max | Default | Unit |
---|---|---|---|---|---|---|---|
Settings | Protection | Enabled Protections A | U1 | 0x00 | 0xFF | 0xA1 | Hex |