SLUS688H March 2006 – November 2015 BQ24120 , BQ24123 , BQ24125
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The bq2412x battery charger supports precision Li-ion or Li-polymer charging system for single cell or two cell application. The design example below shows the design consideration for a 1-cell application.
For this design example, use the parameters listed in Table 2.
DESIGN PARAMETER | EXAMPLE VALUE |
---|---|
AC adapter voltage (VIN) | 16 V |
Battery charge voltage (number of cells in series) | 4.2 V (1 cell) |
Battery charge current (during fast charge phase) | 1.33 A |
Precharge and termination current | 0.133 A |
Safety timer | 5 hours |
Inductor ripple current | 30% of fast charge current (0.4 A) |
Charging temperature range | 0°C to 45°C |
This section provides a detailed system design example for the bq24120.
Set the output inductor to standard 10 μH. Calculate the total ripple current with using the 10 μH inductor:
Calculate the maximum output current (peak current):
Use standard 10 μH inductor with a saturation current higher than 1.471A. (that is, Sumida CDRH74-100)
Use standard value 10 μF, 25V, X5R, ±20% ceramic capacitor (that is, Panasonic 1206 ECJ-3YB1E106M)
In order to get better current regulation accuracy (±10%), let VRSNS be between 100 mV and 200 mV. Use VRSNS = 100 mV and calculate the value for the sense resistor.
This value is not standard in resistors. If this happens, then choose the next larger value which in this case is 0.1Ω. Using the same equation (15) the actual VRSNS will be 133mV. Calculate the power dissipation on the sense resistor:
Select standard value 100 mΩ, 0.25W 0805, 1206 or 2010 size, high precision sensing resistor. (that is, Vishay CRCW1210-0R10F)
Select standard value 7.5 kΩ, 1/16W ±1% resistor (that is, Vishay CRCWD0603-7501-F)
Select standard value 7.5 kΩ, 1/16W ±1% resistor (that is, Vishay CRCWD0603-7501-F)
Select standard value 100 nF, 16V, X7R, ±10% ceramic capacitor (that is, Panasonic ECJ-1VB1C104K). Using this capacitor the actual safety timer will be 4.3 hours.
Assuming a 103AT NTC Thermistor on the battery pack, determine the values for RT1 and RT2 using the following equations:
The bqSWITCHER provides internal loop compensation. With this scheme, best stability occurs when LC resonant frequency, fo is approximately 16 kHz (8 kHz to 32 kHz). Equation 22 can be used to calculate the value of the output inductor and capacitor. Table 3 provides a summary of typical component values for various charge rates.
CHARGE CURRENT | 0.5 A | 1 A | 2 A |
---|---|---|---|
Output inductor, LOUT | 22 μH | 10 μH | 4.7 μH |
Output capacitor, COUT | 4.7 μF | 10 μF | 22 μF (or 2 × 10 μH) ceramic |
Sense resistor, R(SNS) | 0.2 Ω | 0.1 Ω | 0.05 Ω |
Using bq24125 to charge a LiFePO4 battery
The LiFePO4 battery has many unique features such as a very high thermal runaway temperature, high discharge current capability, and high charge current. These special features make it attractive in many applications such as power tools. The recommended charge voltage is 3.6 V and termination current is 50 mA. Figure 23 shows an application circuit for charging one cell LiFePO4 using bq24105. The charge voltage is 3.6 V and recharge voltage is 3.516 V. The fast charging current is set to 1.33 A while the termination current is 50 mA. This circuit can be easily changed to support two or three cell applications. However, only 84 mV difference between regulation set point and rechargeable threshold makes it frequently enter into recharge mode when small load current is applied. This can be solved by lower down the recharge voltage threshold to 200 mV to discharge more energy from the battery before it enters recharge mode again. See the application report, Using the bq24105/25 to Charge LiFePO4 Battery, SLUA443, for additional details. The recharge threshold should be selected according to real application conditions.
Figure 24 shows charging a battery and powering system without affecting battery charge and termination.
The bqSWITCHER was designed as a stand-alone battery charger but can be easily adapted to power a system load, while considering a few minor issues.
Advantages:
Other Issues: