SLUS888G JANUARY 2009 – September 2015
PRODUCTION DATA.
It is possible to design a power supply on a single layer board using the UCC28610. Figure 43 and Figure 44 show an example of a typical layout and design, respectively. Proper use of ground planes can solve EMI and thermal problems. For best results, create a quiet ground plane for the components associated with pins 1 through 4. This offers shielding for the control signals. Also, do not extend the ground plane under heat sinks, thermistors or snubbers so that these components do not heat the UCC28610.
NOTE
The reference designators correspond to the components shown in the schematic of Figure 44.