SLUSC39B June 2015 – February 2017 TPS53647
PRODUCTION DATA.
PIN | I/O(1) | DESCRIPTION | |||
---|---|---|---|---|---|
NAME | NO. | ||||
ADDR-TRISE | 28 | I | Voltage divider to VREF pin. A resistor (RADDR-TRISE) connected between this pin and GND sets the 3-bits. Bit 2 and bit 1 set the rise slew rate. Bit 0 Selects the LSB of BOOT voltage. The voltage (VADDR-TRISE) sets 4 bits PMBus address. The device latches these settings when V3R3 powers up. | ||
COMP | 11 | O | Output of the gM error amplifier. Resistors and capacitors connected between this pin and the VREF pin set the compensation. | ||
CSP1 | 3 | I | Positive current sense inputs. Connect to the IOUT pin of TI smart power stages (ex: CSD95372BQ5MC). Tie CSP4, CSP3, or CSP2 to the V3R3 pin according to Table 3 to disable the corresponding phase. | ||
CSP2 | 4 | ||||
CSP3 | 5 | ||||
CSP4 | 6 | ||||
ENABLE | 23 | I | VR enable. 1-V I/O level; 100-ns debounce. | ||
F-IMAX | 32 | I | Voltage divider to VREF pin. A resistor (RF-IMAX) connected between this pin and GND sets the operating frequency of the controller. The voltage level (VF-IMAX) sets the maximum operating current of the converter. The IMAX value is an 8-bit A/D where VF-IMAX = VVREF × IMAX / 255. Both are latched at V3R3 power-up. | ||
GND | 17 | G | Ground pin. | ||
GND | 20 | G | Connect these pins to GND. Note this is not IC ground pin. | ||
22 | |||||
IMON | 2 | O | Analog current monitor output. ![]() |
||
ISUM | 12 | O | A resistor (RISUM) connected between this pin and VREF pin determines the droop. ![]() (where n is the number of phases) |
||
NC | 7 | — | No connection. Leave the pin open or pull up to V3R3 pin. | ||
8 | |||||
33 | — | No connection. | |||
34 | |||||
OCL-R | 1 | I | A resistor (ROCL-R) connected between this pin and GND and the voltage level (VOCL-R) select 1 of 16 OCL levels (per phase current-limit). VOCL-R also sets one of four RAMP levels. The device latches these settings when V3R3 powers up. | ||
O-USR | 30 | I | Voltage divider to VREF pin. A resistor (RO-USR) connected between this pin and GND selects one of seven OSR thresholds or OFF. The voltage level (VO-USR) sets one of seven USR levels or OFF. The device latches these settings when V3R3 powers up. | ||
PMB_ALERT | 25 | O | I2C PMBus interrupt line. Open drain. 3.3-V and 1.8-V logic level. | ||
PMB_CLK | 24 | I | I2C PMBus clock. 3.3-V and 1.8-V logic level. | ||
PMB_DIO | 26 | I/O | I2C PMBus digital I/O line. 3.3-V and 1.8-V logic level. | ||
PWM1 | 38 | O | PWM signals for each phase | ||
PWM2 | 37 | ||||
PWM3 | 36 | ||||
PWM4 | 35 | ||||
RESET | 21 | I | Reset pin. If this pin is low for more than 1000 ns, the controller pulls the output voltage to the VBOOT level. | ||
SKIP-NVM | 39 | O | A resistor (R SKIP-NVM) connected between this pin and GND sets either pinstrap or NVM configuration mode. This pin can also connect to the FCCM pin of TI smart power stages (ex: CSD95372BQ5MC) for SKIP or FCCM operation. | ||
SLEW-MODE | 29 | I | Voltage divider to VREF pin. A resistor (RSLEW-MODE) connected between this pin and GND sets 8 slew rates. The voltage level (VSLEW-MODE) sets 4-bit operation modes. Bit 7 for DAC mode (1 for VR12.0; 0 for VR12.5). Bit 6 for the 4-phase interleaving mode (1 for 1/3 and 2/4 two phase interleaving; 0 for 4 phase interleaving individually). Bit 4 for enabling dynamic phase add or drop (1 for enable; 0 for disable). Bit 3 sets zero load-line (1 for zero load-line; 0 for non-zero load-line) The device latches these settings when V3R3 powers up. | ||
TSEN | 40 | I | Connect to the TAO/FAULT pin of TI smart power stages (ex: CSD95372BQ5MC) to sense the highest temperature of the power stages and to sense the fault signal from the power stages. | ||
V3R3 | 14 | O | 3.3-V LDO output. Bypass this pin to GND with a ceramic capacitor with a value of 1-µF or larger. | ||
V5 | 15 | P | 5-V power input. Bypass this pin to GND with a ceramic capacitor with a value of 1-µF or larger. This pin is used to power all internal analog circuits. | ||
VBOOT | 31 | I | Voltage divider to VREF pin. A resistor (RVBOOT) connected between this pin and GND sets 3 bits (B[3:1]). The voltage level (VVBOOT) sets 4 bits (B[7:4]). The total 7 bits set 7 of 8 bits of VID of boot voltage (B[7:1]). The device latches these settings when V3R3 powers up. | ||
VIN | 16 | P | Input voltage supply. This pin is also used for input voltage sensing for on-time control and input undervoltage lockout (UVLO). | ||
VR_RDY | 18 | O | Power good open-drain output for the controller. This pin is typically pulled up to V3R3 pin through a resistor with a value of 3-kΩ or larger. | ||
VR_FAULT | 27 | O | VR fault indicator (open-drain). The failures include shorts of the high-side FETs, over temperature, output overvoltage, and overcurrent conditions of the input. The fault signal should be used on the platform to remove the power source either by firing a shunting SCR to blow a fuse or by turning off the AC power supply. When the failure occurs, the VR_FAULT pin is LOW. This pin is typically pulled up to V3R3 pin through a resistor with a value of 3-kΩ or larger. Leave this pin floating if not used. | ||
VR_HOT | 19 | O | Thermal flag open drain output. Active low. This pin is typically pulled up to V3R3 pin through a resistor with a value of 3-kΩ or larger. Leave this pin floating if not used. | ||
VREF | 13 | O | 1.7-V, 500-µA, LDO reference voltage. Bypass this pin to GND with a ceramic capacitor with a value of 0.33 µF. Connect the VREF pin to the REFIN pin of TI smart power stages (ex: CSD95372BQ5MC) as the current-sense reference voltage. | ||
VSN | 10 | I | Negative input of the remote voltage sense amplifier. Connect this pin directly to the GND of the load. | ||
VSP | 9 | I | Positive input of the remote voltage sense amplifier. Connect this pin directly to the load. | ||
Thermal Pad | GND | Thermal pad. Connect the thermal pad to the ground plane with multiple vias. |