SLUSDF8E June 2019 – July 2024
PRODUCTION DATA
Ensure that the output capacitance has enough ripple current rating to absorb the output switching ripple current. Equation 6 shows the output capacitor RMS current ICOUT calculation.
The output capacitor voltage ripple can be calculated as follows:
At certain input and output voltages and switching frequency, the voltage ripple can be reduced by increasing the output filter LC.
The charger device has internal loop compensation optimized for >10-μF ceramic output capacitance. The preferred ceramic capacitor is 10-V rating, X7R or X5R.