SLUUAQ3A April 2016 – October 2022 BQ4050
The BQ4050 detects the BATTERY PACK REMOVED mode if the [NR] bit is set to 0 AND the PRES input is high ([PRES] = 0).
On entry to the BATTERY PACK REMOVED mode, the [TCA] and [TDA] flags are set, ChargingCurrent() and ChargingVoltage() are set to 0, the CHG and DSG FETs are turned off, and the Precharge FET is turned off (if used).
Polling of the PRES pin continues at a rate of once every 1 s.
The BQ4050 exits the BATTERY PACK REMOVED state if the [NR] flag is set to 0 AND the PRES input is low ([PRES] = 1). When this occurs, the [TCA] and [TDA] flags are reset.