SLUUBU0A June 2018 – July 2022 BQ27Z561
The chemistry file contains parameters that the simulations use to model the cell and its operating profile. It is critical to program a Chemistry ID that matches the cell into the device. Some of these parameters can be viewed in the Data Flash section of the Battery Management Studio.
Press the Chemistry button to select the Chemistry window.