SLUUC57B october 2019 – august 2023 BQ79600-Q1
The example code only provides a control interface to the BQ79600-Q1 and BQ79616-Q1 and does not provide any other communications interface to the outside world. The customer is expected to develop their own communication implementation. Examples of communications interfaces available to the TMS570 are SPI, CAN, or UART. For the TMS570 example code, UART is the communication protocol used between the microcontroller and BQ79600-Q1 device.
Importing a project into Code Composer Studio™ :
C:\ti\bq79600-Q1 Example Code 0.1
).
C:\ti\bq79600-Q1 Example Code 0.1