SLUUC57B october 2019 – august 2023 BQ79600-Q1
The EVMs are connected using 4-position Molex connectors. The BQ79600EVM has a high side (J15) and low side (J14) communication connector available on each board. To connect the BQ79600EVM to the BQ79606EVM using NORTH direction for communication, connect J15 on the BQ79600EVM to J5 on the BQ79606EVM. If several BQ79606EVMs are stacked, connect them as indicated in the EVM user's guide for the device. If using ring architecture, connect J6 of the top most BQ79606EVM to J14 on the BQ79600EVM.
Connection Name | BQ79600EVM High Side | BQ79606EVM Low Side |
---|---|---|
COMH_N to COML_N | J15 pin 4 | J5 pin 1 |
COMH_P to COML_P | J15 pin 3 | J5 pin 2 |