The layout of the PoE front end must follow power
and EMI or ESD best-practice guidelines. A basic set of recommendations
includes:
- TI recommends having at least 8 vias (PAD G) and 5 vias on (PAD S) connecting
the exposed thermal pad through a top layer plane (2 oz copper recommended) to a
bottom VSS plane (2 oz. copper recommended) to help with thermal
dissipation.
- The primary MOSFET (Q10 in TPS23730EVM093) must be near the power transformer
and the current sense resistor must be close to source of the MOSFET to minimize
the primary loop. The same is true for the secondary MOSFETs. Keep the MOSFETs
close to the transformer, and associated components as close together as
possible to minimize the loop.
- Parts placement must be driven by power flow in a point-to-point manner; RJ-45, Ethernet transformer, diode bridges, TVS and 0.1-μF capacitor, and TPS23730 converter input bulk capacitor.
- Make all leads as short as possible with wide power traces and paired signal and return.
- No crossovers of signals from one part of the flow to another are allowed.
- Spacing consistent with safety standards like IEC60950 must be observed between the 48-V input voltage rails and between the input and an isolated converter output.
- Use large copper fills and traces on SMT power-dissipating devices, and use wide traces or overlay copper fills in the power path.
- Place the Schotty diode between VSS and RTN as close to the IC as possible, preferably on directly on the opposite side of the board (ex. The TPS23730EVM-093 places the IC on the top side, so the diode is on the bottom side directly underneath it).
The DC-to-DC converter layout benefits from basic rules such as:
- Having at least 4 vias (VDD) near the power transformer pin connected to VDD through multiple layer planes to help with thermal dissipation of the power transformer.
- Having at least 6 vias (secondary ground) near the power transformer pin connected to secondary ground through multiple layer planes to help with thermal dissipation of the power transformer.
- Pair signals to reduce emissions and noise, especially the paths that carry high-current pulses, which include the power semiconductors and magnetics
- Minimize the trace length of high current power semiconductors and magnetic components
- Use the ground plane for the switching currents carefully
- Keep the high-current and high-voltage switching away from low-level sensing circuits including those outside the power supply
- Proper spacing around the high-voltage sections of the converter