SLUUCH2 March 2021 BQ40Z50-R2
The ManufacturerAccess() 0x0081 TMPRead1( ), ManufacturerAccess() 0x0082 TMPRead2( ), ManufacturerAccess() 0x0083 TMPRead3( ) and ManufacturerAccess() 0x0084 TMPRead4( ) read-block commands return the full register array of the TMP468.
The ManufacturerAccess() 0x008B TMPWrite( ) write-word command allows a register to be written with the 1st byte being the TMP468 register pointer (hex) and second byte the data to be written (hex). If the register pointer value received by this command is of a register that is locked or read only then the payload is still sent to the TMP468 even though it will have no impact.