SLUUCH4A October 2021 – October 2023 BQ27Z746
When programming protections in the Protector Threshold sub-window, a trim voltage is needed for reference on the gauge. For where each protector threshold reference voltage should be applied on the EVM, see Figure 6-2.
To set a protection, select the sub-window and use the field adjacent to the protection name to designate a delay or threshold value. Notice the units being used to the right of this field as well as the minimum and maximum values to the left. Click the button on the bottom of the sub-window to program this protection. A green check mark indicates that protector programming was successful.