SLUUCJ6 November 2023
The BQ76907 EVM Quick Start Guide describes connection for basic operation. Providing more than recognizable current in that configuration can require a power supply with a significant power rating. Applying a charge current can damage some power supplies. Figure 4-3 shows a method to force current through the control path without a high wattage power supply or special equipment. The load power supply needs to be set at a low voltage in a constant current mode. Polarity can be reversed on the load supply to simulate a charge current. The battery simulation supply must never be reversed.