All trademarks are the property of their respective owners.
The Texas Instruments LMR54410EVMevaluation module (EVM) helps designers evaluate the operation and performance of the LMR54410 wide-input buck regulator.
EVM Features
The EVM contains one DC/DC converter (see Table 1-1).
CONVERTER | EVM | DEVICE | PACKAGE |
---|---|---|---|
U1 | LMR54410EVM | LMR54410 | SOT23-6 |
This section describes the jumpers and connectors on the EVM and how to properly connect, set up, and use the LMR54410EVM.
VIN — Terminal TP1 – Power input terminal for the converter. Adjacent to it is the GND reference ground. Use this terminal to attach the EVM to a cable harness.
VOUT — Terminal TP3 – Regulated output voltage for the converter. Adjacent to it is the GND reference ground.
GND — Terminal TP2, TP4 – Ground reference for the converter. Use these terminals to attach the EVM to a cable harness.
ENABLE SETTING — Jumper JP1 – Used to enable the switch-mode converter. The device will be enabled when the EN pin is high, and disabled when low.
Testpoint — TP7, TP6, TP9 – Test points used for loop response measurements