SLUUCY1 November   2023

 

  1.   1
  2.   Description
  3.   Features
  4.   Applications
  5.   5
  6. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  7. 2Hardware
    1. 2.1 Configurations and Modifications
      1. 2.1.1 Output Voltage
      2. 2.1.2 Switching Frequency (FSEL Pin)
      3. 2.1.3 Current Limit, Soft-Start Time, and Internal Compensation (MODE Pin)
      4. 2.1.4 Adjustable UVLO
    2. 2.2 Input/Output Connections
    3. 2.3 Best Practices
  8. 3Implementation Results
    1. 3.1 Performance Characteristics Summary
  9. 4Hardware Design Files
    1. 4.1 Schematic
    2. 4.2 PCB Layout
      1. 4.2.1 Layout
    3. 4.3 Bill of Materials
  10. 5Additional Information
    1.     Trademarks

Layout

The board layout for the TPS543B25T is shown in Figure 5-2 through Figure 5-7. The top-side layer of the EVM is laid out in a manner typical of a user application. The top, bottom, and internal layers are 2-oz. copper.

All of the required components for the TPS543B25T are placed on the top layer for U1. The input decoupling capacitors, VDRV capacitor, VCC capacitor, and bootstrap capacitor are all located as close to the IC as possible. Additionally, the voltage set point resistor divider components are kept close to the IC. An additional input bulk capacitor is used near the input terminal to limit the noise entering the converter from the supply used to power the board. Critical analog circuits such as the voltage set point divider, EN resistor, MODE resistor, and FSEL resistor are kept close to the IC and terminated to the quiet analog ground (AGND) island on the top layer.

The top layer contains the main power traces for VIN, VOUT, and SW. The top layer power traces are connected to the planes on other layers of the board with multiple vias placed around the board. There are multiple vias near the PGND pins of the IC to help maximize the thermal performance. Each TPS543B25T circuit has their own dedicated ground are for quiet analog ground that is connected to the main power ground plane at a single point. This single point connection is done on the internal ground planes. Lastly the voltage divider network ties to the output voltage at the point of regulation, the copper VOUT area on the top layer.

The signal layer 1 is a large ground plane and an analog ground island for the MSEL and FSEL resistor and VCC capacitor to connect to by vias. minimize cuts in the ground plane.

The signal layer 2 has VIN copper area beneath each IC to connect the VIN pins together with a low impedance connection. Lastly, the remaining area of this layer is filled in with PGND and additional copper plane for the 2nd stage filter. The mid layer 3 and mid layer 4 is mostly a power ground plane with minimal trace and cuts.

The bottom layer is primarily used for another ground plane. Lastly, the load transient circuit is placed on this side of the EVM.

GUID-20230920-SS0I-WML7-1MVL-JQFJLL1BG1ZH-low.gifFigure 4-2 Top Composite View
GUID-20230920-SS0I-ZFT5-GVCP-2JQHBNRBSKNJ-low.gifFigure 4-4 Signal 2
GUID-20230920-SS0I-FFVL-234F-N0FHRNCZQMGM-low.gifFigure 4-6 Signal 4
GUID-20230920-SS0I-7LQR-ZJ2G-Q7C1SWNSRCSK-low.gifFigure 4-3 Signal 1
GUID-20230920-SS0I-ZGMG-1DVM-Q7ZDR0XXFGDW-low.gifFigure 4-5 Signal 3
GUID-20230920-SS0I-6NLC-CDTR-Z5LZWXT5ZFVP-low.gifFigure 4-7 Bottom Composite View