SLUUCZ1 July 2024 TPS546C25
The EVM has a terminal connection J4 that is used to overdrive the VDRV. The output of the internal regulator is set for 4.5V by default. Using the external supply is useful to minimize the power dissipation in the TPS546C25 IC when operating at high switching frequency. Overdriving the VDRV moves the loss from the internal regulator of the TPS546C25 to the external supply. To use the external supply, follow the steps on the EVM as follows: