Prior to connecting the DC input source, set the current limit of the input supply to 0.1A maximum. Make sure the input source is initially set to 0V and connected to the VIN and GND connection points as shown in Figure 2-1.
Connect ammeter 2 to measure the input current and set to at least 1-second aperture time.