Use the following instructions to
perform the load step test.
- Set the input supply voltage VIN
to 24Vac and current limit of 3A.
- Turn ON the power supply and
observe the rectification of input voltage.
- Once in steady-state, increase
the load using a rheostat.
- Observe the increase in TG1-IN1
and TG2-IN2 voltage levels.
Figure 2-3 shows an example of load step profile captured on the LM74680EVM evaluation
board.