SLVA654B June 2014 – March 2019 DRV8301 , DRV8301-Q1 , DRV8302 , DRV8303 , DRV8307 , DRV8308 , DRV8312 , DRV8323R
The torque loop is used for sensorless applications to control the current through the motor. The torque is related to the current and therefore this feedback measures the current. A sense resistor measures the voltage and current sense amplifier senses the current and sends the signal to the ADC which digitizes the current and sends it to the controller. Measuring the motor current is often used as a safety feature. In case the motor is in a stalled position, the current increases dramatically. Because of this exceptional increase in current, the ADC values reach a current-limit level that causes the system to shut down.