All trademarks are the property of their respective owners.
Brushless-DC (BLDC) motor usage is becoming more and more common for various applications due to the performance benefits they have over alternate motor types such as brushed-DC and stepper motors. As Table 1-1 shows, BLDC motors are more efficient, quieter, and have better power density, higher torque, higher speed, and longer lifetime when compared to brushed-DC and stepper motors.
Motor Type | Pros | Cons |
---|---|---|
Brushless DC | Long life, quiet, optimal power density | Design complexity, higher cost |
Brushed DC | Low cost, easy to use | Noisy, EMI wear-out, sparking |
Stepper | Long life, quiet, open-loop position and speed control | Current control needed, not as power efficient as BLDC, noisy |
The significant benefits that BLDC motors have come with one important disadvantage: higher design complexity. Product development with BLDC motors requires knowledge of how to design an efficient system and get the motor to spin. Texas Instrument’s BLDC team is working to reduce this barrier to entry and simplify BLDC design with innovative motor driver devices. This document serves to simplify BLDC design by exploring the considerations in selecting a BLDC motor driver (Figure 1-1).
The first step in selecting a BLDC driver is to determine what type of architecture is best suited for an application. Architectures range from integrated FET drivers for low- to mid-power applications up to gate drivers enabling multi-kW motor drive systems. In addition, TI’s BLDC portfolio offers integrated control drivers for both sensored and sensorless sinusoidal and trapezoidal control. Figure 2-1 illustrates the various motor driver architectures in TI’s BLDC portfolio such as gate drivers (Blue), integrated FET drivers (Blue + Purple, and sensored vs sensorless integrated control (Green + Blue or Green + Blue + Purple).
Determining supply voltage, output current, and motor power in a system is one of the first steps in selecting what type of motor driver architecture is needed for an application.
Supply voltages come from two categories: battery powered and line powered. In both battery and line powered systems, the supply can vary in voltage, so a motor driver should support at least the maximum voltage of the battery with extra headroom in the case of voltage feedback or transients in the system. TI recommends using a motor driver rated up to 1.2 × the maximum voltage for well-regulated supplies and low-power motors, and 1.5 to 2 times for high-power motors and battery systems. Texas Instruments has a wide-ranging portfolio of motor drivers that support up to 56-V battery systems.
In general, integrated versus external FET architectures have different power requirements. High power (> 70W) systems use gate drivers and low-to-mid-power systems (< 70W) use integrated FET drivers. External FETs are able to drive higher power than integrated FETs because they are not constrained by the size of the single-chip integrated FET driver device. For integrated FET solutions, peak current, RMS current, and RDS(on) of the internal FETs are important considerations that directly relate to the motor power. For external FET solutions, the RDS(on) and current ratings of the external MOSFETs relate to the power the motor can drive.
Table 2-1 compares the specifications of gate driver and integrated FET driver architectures.
Gate Driver | Integrated FET Driver | |
---|---|---|
Power | High power (typically > 70W) | Low to mid power (typically < 70W) |
Voltage Range | Up to 100 V | Normally 60 V or less |
Gate Driver Current | Greater than 3.5-A/4.5-A of source/sink current | - |
Peak Current | - | Up to 13-A |
MOSFETs | External | Internal |
Thermal | Power is dissipated in external MOSFETs | Limited by the size of the integrated package |
Solution Size | Larger | Smaller |